Setting time manually

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting time manually

1,997 Views
Shanga
Contributor III

Hi NXP,

Android 13 imx-android-13.0.0_1.2.0

Method 1 : Update automatically

UI -> Setting -> system-> date&time -> select time zone
1) Enable Set time automatically enabled
2) Connected to internet &   Select time zone  time and date updated and   is retained on cold boot and reboot.

Method 2: Update Manually

Time does not retain when we update time.
when we Set Date and Time manually using HDMI UI.
Setting -> system-> date&time
Time and date are updated ;Reflected on Android UI; but  the system time reverts to the default during cold boot and reboot.
Please share your input how to retain time

IMX8MPLUS  #ANDROID13

Tags (1)
0 Kudos
Reply
3 Replies

1,954 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Shanga 

Setting time manually on i.MX8MP EVK board, the time can be saved after rebooting board.

The test is based on Android 13.0.0_2.2.0. Could you test same version?


Best Regards
Zhiming

0 Kudos
Reply

1,935 Views
Shanga
Contributor III
Hi @Zhiming_Liu
Time retains when only time is changed ,it doesn't retain if any date is changed along with time on Android 13.0.0_2.2.0(if we set time only manually).
0 Kudos
Reply

1,887 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Shanga 

I also changed the date and time without opening setting time automatically and connecting ethernet, the date and time will be  retained after reboot.

Before reboot, the time is 9.14 AM, MON OCT 28

Zhiming_Liu_1-1730078298463.png

 

After reboot, the time is 9.15 AM, MON OCT 28

Zhiming_Liu_0-1730078213713.png

Best Regards
Zhiming

0 Kudos
Reply