Setting the local alpha blending

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting the local alpha blending

ソリューションへジャンプ
5,519件の閲覧回数
valentinryzhenk
Contributor II

Hello,

I faced with a problem when setting the local alpha blending.

Use 2 framebuffer:

fb0 for my qt application (widget with a black background and green text information);

fb1 for outputting a video camera using gstreamer 1.0

How to programmatically configure framebuffer on 32 bit?

P.S. Use this article to configure the global alpha blending, but when mixed are black pixels around the green text.

ラベル(3)
1 解決策
4,550件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Valentin

one can check ipu examples on

ipu-examples release notes - v0.1 | NXP Community 

i.MX6: Alpha blending example code | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
4,549件の閲覧回数
yyuan
Contributor III

hello

i also want to do this.   

i want to add qt to video,  qt is fb0 , video is fb1,but video blocks qt.

do you know how to solve it?

thank you 

0 件の賞賛
返信
4,549件の閲覧回数
valentinryzhenk
Contributor II

Hello, here's an example.

0 件の賞賛
返信
4,549件の閲覧回数
yyuan
Contributor III

thank you    Valentin Ryzhenko

i can`t  open the link ,  but  thank you very much.

thank you

0 件の賞賛
返信
4,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Valentin

one can check ipu examples on

ipu-examples release notes - v0.1 | NXP Community 

i.MX6: Alpha blending example code | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------