Setting MAC address on imxull board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting MAC address on imxull board

1,781 Views
Et_MM
Contributor II

Hi,

I am working with a custom board based on the i.MX 6ULL EVK, and I need to permanently set the MAC address for Ethernet to fe:51:11:6c:62:e8. How can I do this using the OTP fuses / burn fuses?"

0 Kudos
Reply
3 Replies

1,718 Views
Et_MM
Contributor II

Thanks for the solution.

0 Kudos
Reply

1,724 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please refer the attachment for reference to fuse and the section <37.5 OCOTP Memory Map/Register Definition > of IMX6ULLRM 

Regards

Harvey

1,095 Views
JesnaK
Contributor I
Thanks for the solution. I will try this.
0 Kudos
Reply