Setting MAC address on imxull board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting MAC address on imxull board

2,669件の閲覧回数
Et_MM
Contributor III

Hi,

I am working with a custom board based on the i.MX 6ULL EVK, and I need to permanently set the MAC address for Ethernet to fe:51:11:6c:62:e8. How can I do this using the OTP fuses / burn fuses?"

0 件の賞賛
返信
3 返答(返信)

2,606件の閲覧回数
Et_MM
Contributor III

Thanks for the solution.

0 件の賞賛
返信

2,612件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please refer the attachment for reference to fuse and the section <37.5 OCOTP Memory Map/Register Definition > of IMX6ULLRM 

Regards

Harvey

1,983件の閲覧回数
JesnaK
Contributor I
Thanks for the solution. I will try this.
0 件の賞賛
返信