Serial port speed for iMX7 Sabre Development Kit board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial port speed for iMX7 Sabre Development Kit board

1,730 Views
victorgomez
Contributor II

Hi!

I tried looking for this information in the NXP documentation, but I could not find it Seems like this is the most basic information NXP has to provide to access its board, and yet it is not easy to find.

What's the baud's rate speed I should use to access the board via serial? I used the mini-USB to USB that comes with it, and when connected to the DEBUG UART, I can see two different ports. None of them works with any speed baud rate,

Thanks a lot!

Labels (1)
0 Kudos
Reply
1 Reply

1,509 Views
igorpadykov
NXP Employee
NXP Employee

Hi Victor

please refer to p.7 i.MX7SDB Quick Start Guide

http://www.nxp.com/assets/documents/data/en/user-guides/SABRESDBIMX7DUALQSG.pdf 

www.nxp.com/iMX7DSABRE

use uboot/linux on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply