Serial logs are visible in display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial logs are visible in display

Jump to solution
1,977 Views
Hrithik
Contributor III

Hi NXP Team,

We are using iMX8MM on Android 11 OS and it uses LVDS bridge based on i2c for display.
While the device boots up, the serial logs(UART logs) get displayed on the display screen.

Attaching picture for reference:

Hrithik_0-1672642135132.jpeg

This is an undesired behaviour and we want to remove this.

Kindly guide us in removing the same.

Thanks

 

0 Kudos
Reply
1 Solution
1,933 Views
Hrithik
Contributor III

Hi @Sanket_Parekh ,

Thanks for the response.
Actually, we figured out that the logs were coming from Kernel as we hadnt defined console and stdout-path in kernel dts files as done in uboot.

Configuring the same in kernel solved the issue.

Regards,
Hrithik

View solution in original post

0 Kudos
Reply
4 Replies
1,934 Views
Hrithik
Contributor III

Hi @Sanket_Parekh ,

Thanks for the response.
Actually, we figured out that the logs were coming from Kernel as we hadnt defined console and stdout-path in kernel dts files as done in uboot.

Configuring the same in kernel solved the issue.

Regards,
Hrithik

0 Kudos
Reply
1,927 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Hrithik 

Issue is resolved. Can I mark this case to close state?

Thanks & Regards

Sanket Parekh

0 Kudos
Reply
1,914 Views
Hrithik
Contributor III
Hi @Sanket_Parekh

Yes, you can close this case.

Thanks,
Hrithik
0 Kudos
Reply
1,935 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Hrithik ,

I hope you are doing well.
 
Please make sure that you defined the console in defargs environment variable in uboot.
 
Please provide me with the output of printenv in u-boot if this doesn't resolve the issue.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply