Serial logs are visible in display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Serial logs are visible in display

跳至解决方案
2,101 次查看
Hrithik
Contributor III

Hi NXP Team,

We are using iMX8MM on Android 11 OS and it uses LVDS bridge based on i2c for display.
While the device boots up, the serial logs(UART logs) get displayed on the display screen.

Attaching picture for reference:

Hrithik_0-1672642135132.jpeg

This is an undesired behaviour and we want to remove this.

Kindly guide us in removing the same.

Thanks

 

0 项奖励
回复
1 解答
2,057 次查看
Hrithik
Contributor III

Hi @Sanket_Parekh ,

Thanks for the response.
Actually, we figured out that the logs were coming from Kernel as we hadnt defined console and stdout-path in kernel dts files as done in uboot.

Configuring the same in kernel solved the issue.

Regards,
Hrithik

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,058 次查看
Hrithik
Contributor III

Hi @Sanket_Parekh ,

Thanks for the response.
Actually, we figured out that the logs were coming from Kernel as we hadnt defined console and stdout-path in kernel dts files as done in uboot.

Configuring the same in kernel solved the issue.

Regards,
Hrithik

0 项奖励
回复
2,051 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Hrithik 

Issue is resolved. Can I mark this case to close state?

Thanks & Regards

Sanket Parekh

0 项奖励
回复
2,038 次查看
Hrithik
Contributor III
Hi @Sanket_Parekh

Yes, you can close this case.

Thanks,
Hrithik
0 项奖励
回复
2,059 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Hrithik ,

I hope you are doing well.
 
Please make sure that you defined the console in defargs environment variable in uboot.
 
Please provide me with the output of printenv in u-boot if this doesn't resolve the issue.
 
Thanks & Regards,
Sanket Parekh
0 项奖励
回复