Serial downloader with UART1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial downloader with UART1

1,543 次查看
hongtao_li
Contributor III

Hi all, 

I am trying to flash the bootloader to imx6ul board in serial downloader mode with UART1.

First, I send the DCD data with SDP command DCD_WRITE, and the response  WRITE_COMPLETE(0x128A8A12) is received.

Then I send the bootloader with SDP command WRITE_FILE, but I cannot receive the response COMPLETE(0x88888888).

If I don't write the DCD, but only the bootloader after power on into serial download mode, the response COMPLETE(0x88888888) can be received.

Can anyone tell me why?

Thanks.

Best regards.

标签 (1)
0 项奖励
回复
3 回复数

1,459 次查看
igorpadykov
NXP Employee
NXP Employee

Hi li

supporting codes for Serial downloader with UART can be found

in usb_loader sources

GitHub - boundarydevices/imx_usb_loader: USB & UART loader for i.MX5/6/7/8 series 

http://variwiki.com/index.php?title=Imx_usb_loader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,459 次查看
hongtao_li
Contributor III

Hi igor,

I find no configuration file for uart, but only for usb, can you show me the configuration file for uart?

Thanks.

Best regards

Hongtao

0 项奖励
回复

1,459 次查看
hongtao_li
Contributor III

Thanks very much.

0 项奖励
回复