Serial Download Protocol (SDP) security

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial Download Protocol (SDP) security

ソリューションへジャンプ
2,740件の閲覧回数
ceggers
Contributor V

IMX6ULL.pdf states on page 314 (Device Configuration Data, Write data command):

If any of the target addresses do not lie within the allowed
region, none of the values are written. The list of allowable
blocks and target addresses for the chip are provided below.

ceggers_0-1632120703192.png

Page 322 describes the SDP protocol. My expectation is, that the "address white list" for the DCD commands must also apply for the SDP commands. But I didn't find this on the documentation.

Q: Is it save to leave the SDP protocol enabled on a secure device (assuming a HAB version where ERR01087 has been fixed)?

 

0 件の賞賛
返信
1 解決策
2,733件の閲覧回数
Yuri
NXP Employee
NXP Employee

@ceggers 
Hello,

  Yes,  it is safe to leave the SDP protocol enabled on a secure device,
assuming ERR01087is fixed.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,734件の閲覧回数
Yuri
NXP Employee
NXP Employee

@ceggers 
Hello,

  Yes,  it is safe to leave the SDP protocol enabled on a secure device,
assuming ERR01087is fixed.

Regards,
Yuri.

0 件の賞賛
返信