Serial Download - Internal Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial Download - Internal Boot

1,858件の閲覧回数
pauloisaia
Contributor I

Hi, I'm working with an IMXRT1050 and I need to make an image writing by the MCUXpresso Secure Provisioning software. To do this, I set the kit startup to serial download. After burning, the image will only run if I manually change boot to internal boot. I would like to know if it is possible to keep the boot in Serial Download, write the image and run the image without manually switching to internal boot

ラベル(1)
0 件の賞賛
返信
1 返信

1,836件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

It is necessary to switch to internal boot to run the image.
There is some exception when you are using MCUXpresoo with a board. You can open a debug session while you are in serial download and the application runs while the debug session is open.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信