Sequence RAM memory RT1051/RT1052

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sequence RAM memory RT1051/RT1052

跳至解决方案
1,430 次查看
rubensjunior
Contributor IV

Hi friends,

I am development a project (RT1052) where I do not have Flash memory. Then, all my code is in RAM memory (internal RAM + external RAM). However, when I put the external RAM in first position, ocuors the bellow error when is executed.

When I put a internal RAM in first position work fine, but not have enough space for save me code.

Please, I need your help!

pastedImage_1.png

CONSOLE MESSAGE:

MCUXpresso IDE RedlinkMulti Driver v10.3 (Feb 7 2019 22:50:02 - crt_emu_cm_redlink build 760)
Found chip XML file in C:/Users/engenharia/Documents/MCUXpressoIDE_10.3.1_2233/workspace_2/MIMXRT1052B_Project_20191106/Debug\MIMXRT1052xxxxB.xml
Reconnected to existing link server
Connecting to probe 1 core 0 (using server started externally) gave 'OK'
Probe Firmware: LPC-LINK2 CMSIS-DAP V5.224 (NXP Semiconductors)
Serial Number: I3FUJ3GU
VID:PID: 1FC9:0090
USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#7&36a63031&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 0 after searching for a good core
debug interface type = Cortex-M7 (DAP DP ID 0BD11477) over SWD TAP 0
processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0
number of h/w breakpoints = 8
number of flash patches = 0
number of h/w watchpoints = 4
Probe(0): Connected&Reset. DpID: 0BD11477. CpuID: 00000C27. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Content of CoreSight Debug ROM(s):
RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)
ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)
ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)
ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)
ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)
ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)
ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)
ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core
ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT
ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU
ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)
NXP: MIMXRT1052xxxxB
DAP stride is 1024 bytes (256 words)
Connected: was_reset=false. was_stopped=false
Awaiting telnet connection to port 3330 ...
GDB nonstop mode enabled
GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.

1 解答
1,327 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
You'll basically need to write and then a script that pokes the appropriate registers to set the SDRAM up before your debug session attempts to download the code into the RAM.
I've attached a script, so please follow the figure to add it before debugging the project.

Have a great day,
TIC

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,328 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Rubens Junior

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
You'll basically need to write and then a script that pokes the appropriate registers to set the SDRAM up before your debug session attempts to download the code into the RAM.
I've attached a script, so please follow the figure to add it before debugging the project.

Have a great day,
TIC

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------