Sensor Interface with Imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensor Interface with Imx6

1,407 Views
prasadadireddy
Contributor I

Dear all,

I am using i.MX6 quad Meissa Board and try to interface Aptina sensor(mt9p031) through CSI parallel interface.

Sensor requires a External clock (Master CLK) which need to supplied from the processor. In my case the master clock of mt9p031 sensor is connected IO_SROBE pin of csi parallel interface Pin-out on the i.MX6 Meissa board. Is there a way to send a clock signal on that pin? if yes, please suggest  modifications required

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

1,327 Views
igorpadykov
NXP Employee
NXP Employee

Hi prasad

meissa board is not nxp board and not supported in nxp software.

May be recommended to apply to vendor tech support for its schematic

and software sources.

For i.mx6q sensor examples one can look at nxp sabre sd board:

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.(REV C5)
SABRE Platform for Smart Devices | NXP 

Linux documentation on

i.MX Software | NXP 

Some third party documentation

https://www.embeddedartists.com/wp-content/uploads/2018/04/Using_Cameras_on_iMX_Developers_Kit.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply