Sending partition shell error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sending partition shell error

907 次查看
gjfme
Contributor II

Hi everyone:

    我在用mfgtool 下载时碰到下面问题(imx6ull  L4.1.15.2.0.0), sendint partition shell failed. 串口log如下, 定位到 空指针在 drivers/usb/gadget/function/fsl_updater.c  437行。 但是不知道为什么会出现这个空指针,请问我该怎么做?

Unable to handle kernel NULL pointer dereference at virtual address 00000008

pgd = 80004000

[00000008] *pgd=00000000

Internal error: Oops: 5 [#1] PREEMPT SMP ARM

Modules linked in:

CPU: 0 PID: 63 Comm: file-storage Not tainted 4.1.15-2.1.0+ #1

Hardware name: Freescale i.MX6 Ultralite (Device Tree)

task: a83197c0 ti: a8408000 task.ti: a8408000

PC is at fsg_main_thread+0x19d0/0x21f8

LR is at fsg_main_thread+0x19d0/0x21f8

pc : [<80459490>]    lr : [<80459490>]    psr: 20000113

sp : a8409ee8  ip : a83197c0  fp : a82f0d34

r10: a82f0d00  r9 : a8408000  r8 : 80a5b548

r7 : a8409f28  r6 : 80a5b530  r5 : 00000000  r4 : a83bad00

r3 : 80a5b568  r2 : 00000001  r1 : 00000000  r0 : 80a5b548

Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 8000406a  DAC: 00000015

Process file-storage (pid: 63, stack limit = 0xa8408210)

Stack: (0xa8409ee8 to 0xa840a000)

9ee0:                   00000001 808dd84c 00000000 00000000 00002800 00000000

9f00: 809c86c0 43425355 ab733800 a83197c0 53425355 c085d000 a8409f54 806f5184

9f20: 00055302 806f19f0 00000000 a83197c0 8005c450 a8409f34 a8409f34 a83afc00

9f40: a82f0d00 00000000 a83afc00 a82f0d00 80457ac0 00000000 00000000 00000000

9f60: 00000000 8004557c 554355c3 00000000 809c3800 a82f0d00 00000000 00000000

9f80: a8409f80 a8409f80 00000000 00000000 a8409f90 a8409f90 a8409fac a83afc00

9fa0: 800454a0 00000000 00000000 8000f468 00000000 00000000 00000000 00000000

9fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

9fe0: 00000000 00000000 00000000 00000000 00000013 00000000 75eb55c3 55d355c3

[<80459490>] (fsg_main_thread) from [<8004557c>] (kthread+0xdc/0xf4)

[<8004557c>] (kthread) from [<8000f468>] (ret_from_fork+0x14/0x2c)

Code: e5b35038 e1550003 03a05000 eb0a687d (e5953008)

g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage

0 项奖励
回复
0 回复数