Selecting i.MX8 EVK 64-bit ARM host platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Selecting i.MX8 EVK 64-bit ARM host platform

1,262 次查看
pandivijayaraj
Contributor I

We are looking for i.MX8 EVK for 64-bit ARM host evaluation purpose.
Have compared i.MX 8MQuad EVK, i.MX 8MMini EVK boards available in market.
Both of these boards don't have a full-size SDIO slot available to interface external WiFi device.
Could you suggest a specific i.MX8 EVK with a standard full-size SDIO card available for user.
Thanks.

标记 (2)
0 项奖励
回复
1 回复

1,212 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pandi Vijayaraj,

As you mentioned, most i.MX8 boards on the market, both NXP’s and from third-parties use micro SD cards and do not come with a full size SD card slot. All boards I’ve seen from Boundary Device, iWave, Variscite and Toradex use the microSD alternative.

The only exception I’ve seen so far would be Phytec. Their phyCORE-i.MX 8M is listed as having a regular SDIO port. I would recommend double checking with them which board or carrier boards have this feature just to be sure before ordering.

https://www.phytec.in/product/system-on-modules/phycore-imx-8m/

My apologies for the inconvenience.

Regards,

0 项奖励
回复