In my app I need to record an alsasrc to mp3 files. When the user clicks a button, a new file should be created.
The problem is that I have a segmentation fault when I add an mfw_mp3encoder to my pipeline when it is running. When I replace the mfw_mp3encoder with an wavenc, everything works fine.
Is it possible that this is a bug in the mp3encoder of freescale?
When I debug the app, this is the gdb backtrace of the error:
#0 0x44715718 in mp3e_flush_bitstream () from /usr/lib/lib_mp3_enc_arm9_elinux.so.2.2.0
#1 0x44702268 in mfw_gst_mp3enc_sink_event (pad=<value optimized out>, event=0x43602180) at mfw_gst_mp3enc.c:448
#2 0x401d806c in gst_pad_send_event (pad=0x13a0d0, event=0x43602180) at gstpad.c:4962
#3 0x401d8900 in gst_pad_push_event (pad=0x13a008, event=0x43602180) at gstpad.c:4818
#4 0x41cda44c in gst_base_transform_sink_event (pad=<value optimized out>, event=0x43602180) at gstbasetransform.c:1710
#5 0x401d806c in gst_pad_send_event (pad=0xf1710, event=0x43602180) at gstpad.c:4962
#6 0x401d8900 in gst_pad_push_event (pad=0xf1648, event=0x43602180) at gstpad.c:4818
#7 0x41dd2cbc in gst_queue_loop (pad=<value optimized out>) at gstqueue.c:1094
#8 0x401f82d8 in gst_task_func (task=0xfe278) at gsttask.c:234
#9 0x401f9be8 in default_func (tdata=<value optimized out>, pool=<value optimized out>) at gsttaskpool.c:70
#10 0x40108d74 in g_thread_pool_thread_proxy (data=<value optimized out>) at gthreadpool.c:265
#11 0x401077bc in g_thread_create_proxy (data=0x140058) at gthread.c:635
#12 0x4025d7cc in start_thread () from /lib/libpthread.so.0#13 0x4033cc08 in clone () from /lib/libc.so.6