Seeking WEC7 API documentation for the MX53 VPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Seeking WEC7 API documentation for the MX53 VPU

ソリューションへジャンプ
2,672件の閲覧回数
wylie
Contributor I

Hi, I'm looking for the "i.MX5x VPU Application Programming Interface Windows Embedded Compact 7 Reference Manual" and "i.MX53 Applications Processor Reference Manual" as referenced in section 28-4 in the i.MX53 ARD Windows Embedded Compact 7 Reference Manual, but oddly I can't seem to find it anywhere in the i.MX53 Software and development tool resources section. Could someone please point me to its location?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,543件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Shane,

Attach you would find both documents,  I can confirm that even you see that the VPU Api Reference Manual mentions it is for the i.MX51 both devices had the same VPU so it applies perfectly in both.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,544件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Shane,

Attach you would find both documents,  I can confirm that even you see that the VPU Api Reference Manual mentions it is for the i.MX51 both devices had the same VPU so it applies perfectly in both.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------