Security Reference Manual for i.MX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security Reference Manual for i.MX7

4,943 Views
eishishibusawa
Contributor III

Dear Sir

I want to ask about the Security Reference Manual for i.MX7.

I can get the Security Reference Manual for i.MX6 form web site.

(Please refer to the attached file "IMX6.PNG".)

On the other hand, I cannot find the Security Reference Manual for i.MX6 on web.

(Please refer to the attached file "IMX7.PNG".)

Q1.

How can I get the manual?

Best Regards,

Eishi SHIBUSAWA

Labels (2)
0 Kudos
Reply
4 Replies

3,998 Views
b1n225
Contributor I

Are there any update for Security Reference Manual for i.MX7 ? Has it been released?

Thank you.

b1n225

0 Kudos
Reply

4,391 Views
eeroheikkinen
Contributor I

I was looking for the same manual - so how long should we prepare to wait?

I the meanwhile, as I'm trying to figure out whether to use i.MX7 or Layerscape LS1020 in our application, is there any white paper or any kind of documentation about the performance that the crypto accelerators of these parts can provide?

BR Eero Heikkinen

0 Kudos
Reply

4,391 Views
Yuri
NXP Employee
NXP Employee

Hello,

 the data regarding performance of the crypto accelerators are not public.

Please create request(s).  

Sales and Support|NXP  

Regards,

Yuri.

0 Kudos
Reply

4,391 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Eishi SHIBUSAWA,

The Security Reference Manual for i.MX7 is not be released by now, please wait.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply