Secure boot on IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure boot on IMX8MP

Jump to solution
344 Views
kartheek
Contributor III

Hi,

I'm new to Secure Boot on the i.MX8M Plus platform. I've been searching for documentation on implementing Secure Boot using Yocto, but haven't found any relevant resources so far.

Are there any guides or documentation available for enabling Secure Boot on i.MX8MP with Yocto? Any suggestions or pointers would be greatly appreciated.

Thank you,

Kartheek

0 Kudos
Reply
1 Solution
321 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @kartheek 

We have a reference about the secure boot with Yocto automation.

Please refer to the section <10.9 Security reference design> of UG10163.pdf 

 

Regards

Harvey

View solution in original post

3 Replies
322 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @kartheek 

We have a reference about the secure boot with Yocto automation.

Please refer to the section <10.9 Security reference design> of UG10163.pdf 

 

Regards

Harvey

229 Views
kartheek
Contributor III

Hi Harvey,

I’ve followed the Security Reference Design (Section 10.9) from UG10163.pdf along with the NXP Code Signing Tool (CST) documentation to successfully generate the required keys and a signed wic image.
Now, I’d like to verify secure boot functionality on the i.MX8MP without programming the eFuses or closing the device.
Could you please share any documentation or guidance related to pre-fuse secure boot verification?

Thanks,

Kartheek

0 Kudos
Reply
213 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi Kartheek,

There are tools contained with the CST. You can refer to the CST User Guide for more details.

But please be note: The hab4_image_verifier tool is intended solely for experimentation and debugging purposes. Under any circumstance, it should not be considered as a proof or validation of a good HABv4 image. For official verification and image integrity checks, proceed with the recommended secure boot procedures, such as using the hab_status command as outlined in the relevant documentation.

The SRK Fuse hash values must be fused to device but not closing the device Before we run "hab_status" to verify. 

 

Regards

Harvey

0 Kudos
Reply