Secure boot i.mx7D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,749件の閲覧回数
llliu
Contributor I

I have closed my device and secured my device ,hab_status shows that Secure boot enabled.I have downloaded a signed u-boot.imx ,but why I can download a no signed boot.img .It's not secure.I think a signed u-boot.imx can't load a no signed boot.img.Can you help me.Thank you!

タグ(1)
0 件の賞賛
返信
1 解決策
2,437件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Boot ROM does not allow to run unsigned U-boot; further responsibility for verifying and running applications

under U-boot belongs to the U-boot. 

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,438件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Boot ROM does not allow to run unsigned U-boot; further responsibility for verifying and running applications

under U-boot belongs to the U-boot. 

Regards,

Yuri.

0 件の賞賛
返信
2,437件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

You already boot up the board in a secure manner using a closed device + a signed u-boot => so this is secure!

The feature is called secure boot :smileyhappy: not "secure every app in every stage".

After you already boot up, you can use any other app to play with, even a non-signed u-boot.

How you started the 2nd u-boot? 

In theory, if the device is closed the u-boot terminal is no longer available for the user. If still available, you can set boot_delay to 0. 

To stop loading a 2nd u-boot via jtag, you can disable the JTAG programming a dedicated fuse for that.

Btw, for full a full secure chain of trust u-boot - Linux, please take a look also to this AN [1]. But again, even in Linux you can load a custom application. After the device is booting up in a secure manner, it's up to you to maintain the system in a secure state.

Best regards,

Marius

[1] https://www.nxp.com/docs/en/application-note/AN4581.pdf 

0 件の賞賛
返信