Secure boot for mx6sabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Secure boot for mx6sabresd

1,360 次查看
DipinPK
Contributor II

Hi,

I am able to build the u-boot with secure boot feature enabled. But the below command not showing any HAB Block details..

The below is my command for that.

./tools/mkimage -n board/freescale/mx6sabresd/mx6dl_fs053_nt5cc256m16ep-ek-RA_Ver.cfg.cfgtmp -T imximage -e 0x17800000 -d u-boot-dtb.bin u-boot-dtb.imx

and this command shows output like below.

Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 663552 Bytes = 648.00 KiB = 0.63 MiB
Load Address: 177ff420
Entry Point: 17800000.

What is missing for my u-boot?

Why its not showing HAB Blocks?

Used uboot version : 2018.03

Thanks

 

0 项奖励
回复
1 回复

1,316 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复