Secure boot Fuse Registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure boot Fuse Registers

1,098 Views
AKHIL10
Contributor I

I was Working on the secure boot in iMX8DXL. The 16 Fuse values are generated successfully. May i know which register value i should write this 16 SRK fuse values?

0 Kudos
Reply
1 Reply

1,069 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @AKHIL10,

I hope you are doing well.

- Please refer to the SCFW API Reference Guide for complete information regarding the fuse read/write functions and the SC_R_SYSTEM resource. Examples of how to call the SCFW fuse API functions are available in the NXP Board Support Package.
- Please refer to Chapter 7: FuseMap, of i.MX8DX application reference manual.
- Section 7.2 describes details of the various fuses and their associated configuration settings.
 
Thanks and Regards,
Sanket Parekh
0 Kudos
Reply