Secure Provisioning Tool error XIP encrypted (BEE OTPMK) authenticated and HAB disabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure Provisioning Tool error XIP encrypted (BEE OTPMK) authenticated and HAB disabled

1,640件の閲覧回数
mkarandikar
Contributor I

Hi,

I'm following this webinar to learn how to use the Secure Provisioning Tool with an i.MX RT1060 with different types of boot.

As I'm in the learning phase, I'm using the "Open, HAB disabled" life cycle option in the Secure Provisioning Tool (version 4.0.1)

But when I try and use the last boot type demo'd in the webinar which is XIP encrypted (BEE OTPMK) authenticated with the life cycle selected as Open, HAB disabled I get this error in the Log 

"It is not possible to create encrypted image with disabled security" (see attached image of error)

Can someone help me understand why this is? 

If it helps I'm using and MIMXRT1060-EVKB.

 

ラベル(2)
0 件の賞賛
返信
0 返答(返信)