Searching Target-Config-File for OpenOCD and IMX6QP (Plus!)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Searching Target-Config-File for OpenOCD and IMX6QP (Plus!)

2,034 次查看
martin_maurer
Contributor III

Hello,

has someone already used OpenOCD together with IMX6QP (or any other IMX6 "Plus" version)?

The IMX6QP has different IDs, I already adapted them. Do I need other changes?When doing a reset, it always tells me "How to reset?". How can I solve this?

I am using an Olimex ARM-USB-OCD-H and IMX6QP SABRE board, OpenOCD (0.9.0).

Best regards,

Martin

标签 (1)
0 项奖励
回复
3 回复数

1,574 次查看
prathamrahate
Contributor III

Hi Martin,

What are the JTAG ID you have used for i.MX6qp ?? I am also trying to connect openocd 0.8.0 to imx6qp board, but i am getting below error.

Error: JTAG scan chain interrogation failed: all zeroes
Error: Check JTAG interface, timings, target power, etc.
Error: Trying to use configured scan chain anyway...
Error: imx6.dap: IR capture error; saw 0x00 not 0x01
Warn : Bypassing JTAG setup events due to errors
Warn : Invalid ACK 0 in JTAG-DP transaction

Thanks,

Prathamesh Rahate.

0 项奖励
回复

1,574 次查看
sinanakman
Senior Contributor III

Hi Martin

You might also try posting your question to openocd mailing list or

ask at #openocd chat room. I had ordered the MCIMX6QP-SDB

board, when I receive I'll work on an openocd config.

Regards

Sinan Akman

0 项奖励
回复

1,574 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

unfortunately I am not aware of OpenOCD configurations

working together with IMX6QP, it may be recommended to apply to

NXP Professional Services for developing it:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Pro-Support contact www.nxp.com/prosupport

Best regards

igor

0 项奖励
回复