Search commandline transfer tool for iMx28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Search commandline transfer tool for iMx28

1,405件の閲覧回数
fehrlest
Contributor I

I use the MfGTool 1.6 to transfer the Windows CE-Image inkl. the eboot to the embedded module during the development.

Now I search a commandline tool for the series production, but I did not find anyone.

I found only the "sb_loader.exe", but I cannot transfer the eboot.

Is there a tool for the iMx28 like the MFGtool2?

ラベル(2)
0 件の賞賛
返信
1 返信

1,187件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Stefan

in general MFGtool2 was developed for i.MX6, however

preliminary mfgtools-rel_1.6.2.055 (Mfg tool for i.MX28 not support USB3.0 )

seems supports i.MX28. One can try it.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信