SI configuration in DDR Stress test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SI configuration in DDR Stress test

949 次查看
srinivasaporam
Contributor II

Hi,

Can anybody tell me how the SI configuration bits need to be selected correctly, so that i will generate correct .inc file.

 

DRAM DSE Setting - DQ/DQM (ohm)
DRAM DSE Setting - ADDR/CMD/CTL (ohm)
DRAM DSE Setting - CK (ohm)
DRAM DSE Setting - DQS (ohm)

selecting them in trial and error method will be tedious.

标签 (4)
标记 (1)
0 项奖励
回复
1 回复

834 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

one can find in which direction to change drive strength,

slightly changing temperature. If cooling down the part causes more failures,

then it is likely the drive strength is too high causing more overshoots and undershoots.

If heating up the part causes more failures, then the drive strength is too low

and the signals may not rise/fall fast enough.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复