Screen refresh timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Screen refresh timing

ソリューションへジャンプ
2,145件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

From i.MX 6Solo/6DualLite Applications Processor Reference Manual, Rev. 4, 07/2018

38.1.2.1.6.1 Screen Refresh
• The refresh rate may vary within a predefined range. Within this range, the rate is
dynamically adjusted to the content update rate.

Reference manual mentioned that IPU will change display's refresh rate dynamically.

Let me confirm two things with you.

Q1. What is meaning of above description? I suppose if DMFC has not updated every frame, refresh rate will be down. is it right?

Q2. How do I know current refresh rate? does any register indicate us the current refresh rate?

Best Regards,

Kazuma Sasaki.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,036件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kazuma Sasaki,

My apologies for the delay.

I was reviewing the screen refresh characteristics and (Q1) the refresh rate is adjusted according to the HSYNC, VSYNC and pixel clock, which determines the resolution of the frame. It is not dependent on the content itself (unlike a decoder, for example, that optimizes compression depending on how much the content changes from frame to frame).

As for how to know the current refresh rate (Q2) there is not a register that has the refresh rate although you could calculate it from the display parameters.

I hope this information helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,037件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kazuma Sasaki,

My apologies for the delay.

I was reviewing the screen refresh characteristics and (Q1) the refresh rate is adjusted according to the HSYNC, VSYNC and pixel clock, which determines the resolution of the frame. It is not dependent on the content itself (unlike a decoder, for example, that optimizes compression depending on how much the content changes from frame to frame).

As for how to know the current refresh rate (Q2) there is not a register that has the refresh rate although you could calculate it from the display parameters.

I hope this information helps!

Regards,

0 件の賞賛
返信
2,036件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hello gusarambula,

Okay, I got it. I appreciate your support.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信