Screen is truned off automatically.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Screen is truned off automatically.

1,556件の閲覧回数
yifonglin
Contributor II

Dear All:

I put a picture in screen by framebuffer, but the screen is turned off automatically after several minutes, and no any information is showed in console.

But the screen does not be turned off when QT is runing.

Does someone know what problem is it?

How do I disable the screen auto turn off function?

Thank you.

3 返答(返信)

1,392件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to the following thread .

Linux IMX53 - Console / screen blanking...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,392件の閲覧回数
yifonglin
Contributor II

Hi Yuri:

Thank you to provide a nice reference link, it has solved my problem.

But "Correct Button" does not appear in this thread. I don't know why.

It's very strange. :smileyconfused:

YiFong

0 件の賞賛
返信

1,392件の閲覧回数
Yuri
NXP Employee
NXP Employee

Do not worry !

~Yuri.

0 件の賞賛
返信