Hi
running bare metal, I have a loader that loads code at 0x17800000 .. cf uboot.
I need a serial debug port asap, so want to set it up BEFORE turning any mmu stuff on. This means I have to set up all relevant clock.pad.mux, etc settings, as well as the actual uart.
The assembler I use for this is below. Can anyone suggest what I've missed? Please assume I've set the base addresses to the correct values for physical addresses
Thanks in advance (& is equivalent to 0x)
HAL_UARTStartUp
; first setup pads,pins, and clock sources
ldr a2, [sb, #:INDEX:IOMUXC_Base]
ldr a3, =0x1b0b0 ; pad drive stuff
str a3, [a2,#IOMUXC_SW_PAD_CTL_PAD_EIM_D19-IOMUXC_BASE_ADDR] ; cts
str a3, [a2,#IOMUXC_SW_PAD_CTL_PAD_EIM_D20-IOMUXC_BASE_ADDR] ; rts
str a3, [a2,#IOMUXC_SW_PAD_CTL_PAD_CSI0_DAT10-IOMUXC_BASE_ADDR]
str a3, [a2,#IOMUXC_SW_PAD_CTL_PAD_CSI0_DAT11-IOMUXC_BASE_ADDR]
mov a3, #3 ; alt3
str a3, [a2,#IOMUXC_SW_MUX_CTL_PAD_CSI0_DAT10-IOMUXC_BASE_ADDR] ;txd
str a3, [a2,#IOMUXC_SW_MUX_CTL_PAD_CSI0_DAT11-IOMUXC_BASE_ADDR] ;rxd
mov a3, #1 ;UART1_UART_RX_DATA_SELECT_INPUT
str a3, [a2,#IOMUXC_UART1_IPP_UART_RXD_MUX_SELECT_INPUT-IOMUXC_BASE_ADDR]
str a3, [a2,#IOMUXC_UART1_IPP_UART_RTS_B_SELECT_INPUT-IOMUXC_BASE_ADDR]
ldr a2, [sb, #:INDEX:CCM_Base]
; root clock o/p to uart
ldr a3, [a2,#CCM_CSCDR1_OFFSET]
bic a3, a3, #&3f ; ensure uart_podf set to 1
str a3, [a2,#CCM_CSCDR1_OFFSET]
; turn on uart clock supply
ldr a3, [a2,#CCM_CCGR5_OFFSET]
orr a3, a3, #&f<<24 ; ensure uart clock and serial clock on
str a3, [a2,#CCM_CCGR5_OFFSET]
; now set uart registers up
BaseAddr
mov a2, #1 ;reset UART state machines
str a2, [a1, #UART_UCR2_OFFSET]
mov a2, #&60<<8
add a2, a2, #&66 ;UCR2 = 8n2,IRTS,CTSC,TXEN,RXEN=1,reset clr
str a2, [a1, #UART_UCR2_OFFSET]
mov a2, #1 ;UARTEN = 1,enable the clock
str a2, [a1, #UART_UCR1_OFFSET]
mov a2, #0x4
str a2, [a1, #UART_UCR3_OFFSET] ;set RXD_MUX_SEL bit
ldr a2, [a1, #UART_UFCR_OFFSET]
bic a2, a2, #7<<7
orr a2, a2, #5<<7 ;set RFDIV to div-by-1 or b101
str a2, [a1, #UART_UFCR_OFFSET]
mov a2, #0x4
str a2, [a1, #UART_UBIR_OFFSET]
mov a2,#0xd8
str a2, [a1, #UART_UBMR_OFFSET]
MOV pc, lr