Sample source of DDR bus clock change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample source of DDR bus clock change

ソリューションへジャンプ
1,602件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm using i.MX6SL with Linux Yocto and want to change DDR3's bus clock for sysytem evalutation.

I found some sources in BSP such as busfreq-imx6.c、busfreq-ddr3.c and busfreq-lpddr2.c.

However, I think those files are for i.MX6Q/D/DL/SL.

Does anyone have a sample source for i.MX6SL ?

If anyone doesn't have sample source, please teach me where I should change.

Ko-hey

ラベル(3)
0 件の賞賛
返信
1 解決策
1,340件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

one can try to refer to the patch for L3.0.35

<i.MX6SL DDR3 support for L3.0.35_2.1.0 >.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,341件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

one can try to refer to the patch for L3.0.35

<i.MX6SL DDR3 support for L3.0.35_2.1.0 >.

0 件の賞賛
返信
1,340件の閲覧回数
ko-hey
Senior Contributor II

Hi Guanqiong Xie

Thanks.

I'll try it.

Ko-hey

0 件の賞賛
返信