Sample code to use i.MX6DQ EIM burst access.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sample code to use i.MX6DQ EIM burst access.

跳至解决方案
2,824 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6DQ EIM.

They want to know where is the sample code to use EIM burst read / write.

Is there some sample?

Especially, I will appreciate if you teach me where is the code to use EIM burst write when BL (chapter 22.9..1 in IMX6DQRM Rev.2) = 100 (Continuous burst length).

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (1)
1 解答
2,103 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am not aware of such examples, however I think one can use attached i.MX53 example

and modify it for i.MX6 using i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,103 次查看
bipin7301
Contributor II

Hi @satoshishimoda 

I was also trying to do similar kind of thing but in i.MX7.

 

Were you able to achieve what you were trying to do ?

 

Can you please share your understanding/coding details ?

 

Regards

Bipin Kumar

0 项奖励
回复
2,104 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am not aware of such examples, however I think one can use attached i.MX53 example

and modify it for i.MX6 using i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复