Sabresd IMX7 development board with pre-mounted eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabresd IMX7 development board with pre-mounted eMMC

1,626件の閲覧回数
gopinathsriniva
Contributor III

Hi All,

I want to know, Can I get sabresd IMX7 board with pre-mounted eMMC memory chip? If so can anyone send me those details? 

Thank You in advance. 

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,498件の閲覧回数
art
NXP Employee
NXP Employee

The eMMC memory chip should be pre-mounted on the board. Please check the U10 ref. des. on the PCB.


Have a great day,
Artur

0 件の賞賛
返信

1,498件の閲覧回数
gopinathsriniva
Contributor III

Hi Artur,

I have brought an MCIMX7SABRE from vendor name "Mouser" , where I cannot find any pre-mounted eMMC memory chip. Please see the below image of board. Even the use manual is saying, only eMMC expansion will be present. 

IMG_20170531_192352126.jpg

Can you please say the part number of sabreSD board which will have pre-mounted eMMC? 

0 件の賞賛
返信