Sabrelite from boundary device doesn't play video in dual display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabrelite from boundary device doesn't play video in dual display

998 Views
__ka
Contributor I

Hi,

       I purchase that board from boundary device version : rev-D 5-9-12 and I want to connect dual display (HDMI, LCD)
I have some question to ask.
1. First Question Why the demos shipped with the board doesn't work, It's not show any thing on HDMI but when i changed the kernel it's can show

timesys demo on HDMI but can't play video with VPU decode please check you demo with HDMI.


2. Second Question I build rootfs and kernel byself with LTIB and put on that board it's look working on primary display but i have some trouble on second display

setenv bootargs $bootargs video=mxcfb0:dev=hdmi,1270x720M@60,if=RGB24

setenv bootargs $bootargs video=mxcfb1:dev=lcd,CLAA-WVGA,if=RGB24

setenv fbmem "fbmem=28M,10M";


Then I played video with command :

gst-launch playbin2 uri=file:///home/TestVideo1.mp4 video-sink="mfw_v4lsink device=/dev/video17" &

gst-launch playbin2 uri=file:///home/TestVideo2.avi video-sink="mfw_v4lsink device=/dev/video19"

first Video it's work fine on primary display but second video can't show on LCD screen and when I swap LCD and HDMI with command
setenv bootargs $bootargs video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB24

setenv bootargs $bootargs video=mxcfb1:dev=hdmi,1270x720M@60,if=RGB24

setenv fbmem "fbmem=10M,28M";


LCD look work fine.


Labels (3)
0 Kudos
Reply
0 Replies