SabreSDP Android N tag/branch missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SabreSDP Android N tag/branch missing

2,351件の閲覧回数
vijaikumar
Contributor III

Hi All,

I was trying to setup Android N for SabreSD using Android User Manual from Freescale. However, I was not able to locate the tag/branch n7.1.1_1.0.0-ga. Is the Git server not updated with the tag/branch?

Thanks,

Vijai Kumar K

ラベル(7)
0 件の賞賛
返信
3 返答(返信)

2,248件の閲覧回数
danwei_luo
NXP Employee
NXP Employee

Hi Vijai,

Are you talking about kernel git repository or u-boot git repository?

If you are referring to the kernel, then you can find n7.1.1_1.0.0-ga branch in this git :

linux-imx.git - i.MX Linux Kernel 

As for the u-boot, you can find the n7 branch in this git:

uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards,

Danwei

2,248件の閲覧回数
vijaikumar
Contributor III

Thank You danweiluo‌. I have been searching for it in linux-2.6-imx.git - Freescale i.MX Linux Tree . So from now on linux-imx.git - i.MX Linux Kernel is the official tree?

0 件の賞賛
返信

2,248件の閲覧回数
danwei_luo
NXP Employee
NXP Employee

Yes, that's right!

0 件の賞賛
返信