SabreSDP Android N tag/branch missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SabreSDP Android N tag/branch missing

2,357 Views
vijaikumar
Contributor III

Hi All,

I was trying to setup Android N for SabreSD using Android User Manual from Freescale. However, I was not able to locate the tag/branch n7.1.1_1.0.0-ga. Is the Git server not updated with the tag/branch?

Thanks,

Vijai Kumar K

0 Kudos
Reply
3 Replies

2,254 Views
danwei_luo
NXP Employee
NXP Employee

Hi Vijai,

Are you talking about kernel git repository or u-boot git repository?

If you are referring to the kernel, then you can find n7.1.1_1.0.0-ga branch in this git :

linux-imx.git - i.MX Linux Kernel 

As for the u-boot, you can find the n7 branch in this git:

uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards,

Danwei

2,254 Views
vijaikumar
Contributor III

Thank You danweiluo‌. I have been searching for it in linux-2.6-imx.git - Freescale i.MX Linux Tree . So from now on linux-imx.git - i.MX Linux Kernel is the official tree?

0 Kudos
Reply

2,254 Views
danwei_luo
NXP Employee
NXP Employee

Yes, that's right!

0 Kudos
Reply