SabreSD: PCIe Endpoint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SabreSD: PCIe Endpoint

ソリューションへジャンプ
4,194件の閲覧回数
farhanmasood
Contributor II

I am trying to connect SabreSD as an endpoint to a PC. I followed i.MX6Q PCIe EP/RC Validation System and i.MX6Q: Using an external reference for PCIe for building the kernel image. I set clkdiv2 and mpll to accept 100Mhz external clock.

when I connect it with a PC, PC says PCIe link initialization failed. With internal reference, EP works fine with a Sabrelite RC. Please help!!!

ラベル(1)
1 解決策
3,838件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,839件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
3,838件の閲覧回数
b47504
NXP Employee
NXP Employee

I would suggest you should make sure the external clock can work correctly firstly, then tried it with PC. 

3,838件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Farhan

does it work with internal reference with PC RC ?

Best regards

igor

0 件の賞賛
返信
3,838件の閲覧回数
farhanmasood
Contributor II

no it doesnt :smileysad:

0 件の賞賛
返信
3,838件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Farhan

suggest to check if TX lines on PC side have in series 0.1uF capacitors as C6,C5

in SPF-27392 p.16

SABRE Platform for Smart Devices Reference Design Based on the i.MX 6 Series 

~igor

0 件の賞賛
返信
3,838件の閲覧回数
farhanmasood
Contributor II

Yes there are caps on both Tx lines. None on Rx lines.

0 件の賞賛
返信
3,838件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I think you can try several PCs, seems noise (more on PC

than on i.MX6 RC board) greatly affects connection.

You can check posts from key two with SABRE Lite board,

checking link with ./memtool -32 01ffc72c and trying different cables

i.MX6Q PCIe EP/RC Validation System

~igor

0 件の賞賛
返信