Sabre table operation using 2 cell battery instead of 3 cell

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre table operation using 2 cell battery instead of 3 cell

813件の閲覧回数
erwinw
Contributor III

On the Sbare tablet for i.mx53, would like to change the battery pack to a 2-cell, 7.4V pack. Can someone tell us what would be the implications on the Sabre platform to doing this?  It is easy enough to change the number of cell setting for the MAX1705B charger, but  need to know what other implications or modifications there would be.

タグ(2)
0 件の賞賛
返信
0 返答(返信)