Sabre Smart Devices RAM Adress Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre Smart Devices RAM Adress Pins

Jump to solution
2,965 Views
atillametetured
Contributor V

Hello

Quick question about the RAM schematioc of Sabre. Oddly, adress pins A15 and A14 are seen as NC pins and on the RAM side they are not connected to the bus but on the imx side they are. Why is it in this matter? Below are the snips from the Sabre Ram schematic;

Memory side;

RAMQUestion.PNG

i.MX side;

RAMQUestion2.PNG

Thanks in advance and best regards,

Mete

Labels (2)
Tags (5)
0 Kudos
Reply
1 Solution
2,673 Views
BiyongSUN
NXP Employee
NXP Employee

Yes, this design can fit row A[15:0].

i.MX6 side row is [15:0] is greater than the DDR device 128Mx16 [13:0]. The [15:14] is not used.

But if we want to use  256MX8. the row is [14:0]. i.MX6 side still can handle cause the A14 is connect.

You just uninstall the device 128Mx16 and install the device 256MX8.

If the design on i.MX6 side is like this.  A14 and A15 is not connected, then we could not switch the device to 256MX8, because the A14 is really NC.

View solution in original post

4 Replies
2,673 Views
BiyongSUN
NXP Employee
NXP Employee

mt41k128m16jt  has three parts with the same package.

The 128Mx16 the row is only  [13:0]. It is easy to replace with the another part. Even the part needs row [15:0].

If the i.MX6 side is NC, too. The design has no chance to switch to new part like 256MX8.

Untitled.png

0 Kudos
Reply
2,673 Views
atillametetured
Contributor V

What about 512MX16? Can the design swithc to that? Sorry have a bit hard time udnerstanding the language. So the design implies that Sabre only uses A[13:0] but is designed to fit A[15:0]. Is this what you mean?

0 Kudos
Reply
2,674 Views
BiyongSUN
NXP Employee
NXP Employee

Yes, this design can fit row A[15:0].

i.MX6 side row is [15:0] is greater than the DDR device 128Mx16 [13:0]. The [15:14] is not used.

But if we want to use  256MX8. the row is [14:0]. i.MX6 side still can handle cause the A14 is connect.

You just uninstall the device 128Mx16 and install the device 256MX8.

If the design on i.MX6 side is like this.  A14 and A15 is not connected, then we could not switch the device to 256MX8, because the A14 is really NC.

2,673 Views
atillametetured
Contributor V

Okay thanks Biyong.

Regards,

Mete

0 Kudos
Reply