Sabre SD board DDR3 Address timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre SD board DDR3 Address timing

1,449件の閲覧回数
sparkyee
Contributor I

Hi,

    Does anyone know if the Sabre for smart Devices reference board was designed

for 1T or 2T DDR3 Address Timing? I am trying to do a Hyperlynx simulation of the

board and need to know how to setup the timing. Any help is appreciated!

Thanks!

Larry

ラベル(4)
0 件の賞賛
返信
1 返信

1,299件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  There is no special mode for the 2T ; all timing parameters may be configured via MMDC registers, no more.

For more detailed configuring, please use the following tool.

i.MX6DQ SABRE SDP/B DDR3 Register Programming Aid

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信