Sabre Lite Terminal Keyboard Input Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre Lite Terminal Keyboard Input Error

2,225 Views
chrisgeilker
Contributor I

Hi,

I have a problem with the Temrinal emulation (putty) with my Sabre Lite board.

The output from the boot process ist correct, but I can`t make any input...

The OS on my PC ist Windows 7 64-bit

The settings of the terminal emulation seems to be okay:

115.2 kbaud, 8 data bits, 1 stop bit, no parity, no flow control.

I have used the cables from the kit: 1 Custom Serial cable, 6-pin female to dual DB9 mal connectos an 1 DB9 female to DB9 female cable.

What ist wrong? Where is my mistake?

Many thanks,

Chris

Labels (1)
0 Kudos
Reply
3 Replies

2,003 Views
EricNelson
Senior Contributor II

Hi Chris,

Your settings are correct (115200,8,N,1, no flow control).

The dual-DB-9 to Molex cable we ship is configured as DCE, to allow direct connection to a PC serial port or USB serial adapter.

I'm not sure what you're referring to regarding the DB9 female-female cable and the "custom serial cable".

Can you take a photo?

From your description of the symptoms, it appears that the Tx line from your PC isn't making it to the board.

0 Kudos
Reply

2,003 Views
chrisgeilker
Contributor I

The DB9 cable  ist a standard serial cable Sub D

The other cable is a Molex to 2 x Sub D (one for Debug).

The Cables ar in the Kit from element14.

Here is the phoIMG_20140301_084439082[1].jpgto:

0 Kudos
Reply

2,003 Views
EricNelson
Senior Contributor II

Hi Chris,

Chris Geilker wrote:d

...

The Cables ar in the Kit from element14.

Then I have no idea how you need to cable things. You might need to put a meter on the cable to verify that pin 3 on your DB-9 from your PC is connected to Pin 5 of J17 on the SABRE Lite.

0 Kudos
Reply