Sabre Lite - Linux Booting.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre Lite - Linux Booting.

3,770件の閲覧回数
venkatachilakal
Contributor III

Please help me in this ...

I just followed the this website for sd card preparation and and compiling kernel and copying the filesystem.

I have followed each and every stem in that page to run linux on Sabre Lite with 2014 U-Boot.

But, some where it stuck and it is unable to complete the booting process. And some time booting will be completed and nothing will work. as shown in log.

Please help me where I doing wrong..

Please find the below log for further references.

------------------------------------------------------------------------

U-Boot 2014.04-00123-g63ae4a5 (May 14 2014 - 17:09:55)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

Reset cause: POR

Board: SABRE Lite

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

*** Warning - bad CRC, using default environment

auto-detected panel HDMI

Display: HDMI (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   using phy at 6

FEC [PRIME]

-

5993088 bytes read in 453 ms (12.6 MiB/s)

56913 bytes read in 488 ms (113.3 KiB/s)

Kernel image @ 0x12000000 [ 0x000000 - 0x5b7280 ]

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 18010e50

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Linux version 4.6.3-armv7-x4 (root@hb-HCL-Desktop) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP Wed Jul 13 16:52:20 IST 2016

[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d

[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

[    0.000000] Machine model: Freescale i.MX6 Quad SABRE Lite Board

[    0.000000] cma: Reserved 24 MiB at 0x4e800000

[    0.000000] Memory policy: Data cache writealloc

[    0.000000] percpu: Embedded 14 pages/cpu @ef691000 s24960 r8192 d24192 u57344

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260416

[    0.000000] Kernel command line: console=ttymxc1,115200n8 console=tty0 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait fixrtc video= mxcfb0:dev=hdmi,1280x720M@60,if=RGB24

[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)

[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

[    0.000000] Memory: 990872K/1048576K available (13193K kernel code, 1326K rwdata, 4680K rodata, 2048K init, 802K bss, 33128K reserved, 24576K cma-reserved, 237568K highmem)

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

[    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)

[    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)

[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

[    0.000000]       .text : 0xc0008000 - 0xc12746b8   (18866 kB)

[    0.000000]       .init : 0xc1300000 - 0xc1500000   (2048 kB)

[    0.000000]       .data : 0xc1500000 - 0xc164b85c   (1327 kB)

[    0.000000]        .bss : 0xc164d000 - 0xc1715b9c   ( 803 kB)

[    0.000000] Hierarchical RCU implementation.

[    0.000000]  Build-time adjustment of leaf fanout to 32.

[    0.000000] NR_IRQS:16 nr_irqs:16 16

[    0.000000] L2C-310 erratum 769419 enabled

[    0.000000] L2C-310 enabling early BRESP for Cortex-A9

[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9

[    0.000000] L2C-310 ID prefetch enabled, offset 1 lines

[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled

[    0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB

[    0.000000] L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001

[    0.000000] Switching to timer-based delay loop, resolution 333ns

[    0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns

[    0.000027] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns

[    0.003690] Console: colour dummy device 80x30

[    0.004418] console [tty0] enabled

[    0.004465] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=12000)

[    0.004514] pid_max: default: 32768 minimum: 301

[    0.004731] Security Framework initialized

[    0.004761] Yama: becoming mindful.

[    0.004802] AppArmor: AppArmor disabled by boot time parameter

[    0.005011] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

[    0.005046] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

[    0.005936] CPU: Testing write buffer coherency: ok

[    0.005995] ftrace: allocating 39493 entries in 116 pages

[    0.078489] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

[    0.078637] Setting up static identity map for 0x10100000 - 0x10100098

[    0.085199] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

[    0.086303] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

[    0.087386] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

[    0.087490] Brought up 4 CPUs

[    0.087578] SMP: Total of 4 processors activated (24.00 BogoMIPS).

[    0.087598] CPU: All CPU(s) started in SVC mode.

[    0.088661] devtmpfs: initialized

[    0.105023] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

[    0.105595] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns

[    0.107551] xor: measuring software checksum speed

[    0.147340]    arm4regs  :  1213.000 MB/sec

[    0.187339]    8regs     :   872.000 MB/sec

[    0.227337]    32regs    :   903.000 MB/sec

[    0.267337]    neon      :   877.000 MB/sec

[    0.267361] xor: using function: arm4regs (1213.000 MB/sec)

[    0.267444] pinctrl core: initialized pinctrl subsystem

[    0.269287] NET: Registered protocol family 16

[    0.272568] DMA: preallocated 256 KiB pool for atomic coherent allocations

[    0.283414] cpuidle: using governor menu

[    0.283913] CPU identified as i.MX6Q, silicon rev 1.2

[    0.311596] No ATAGs?

[    0.311643] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

[    0.311692] hw-breakpoint: maximum watchpoint size is 4 bytes.

[    0.313448] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

[    0.314982] Serial: AMBA PL011 UART driver

[    0.407698] raid6: int32x1  gen()   129 MB/s

[    0.475524] raid6: int32x1  xor()   137 MB/s

[    0.543663] raid6: int32x2  gen()   157 MB/s

[    0.611513] raid6: int32x2  xor()   156 MB/s

[    0.679577] raid6: int32x4  gen()   189 MB/s

[    0.747501] raid6: int32x4  xor()   156 MB/s

[    0.815629] raid6: int32x8  gen()   208 MB/s

[    0.883496] raid6: int32x8  xor()   139 MB/s

[    0.951435] raid6: neonx1   gen()   613 MB/s

[    1.019359] raid6: neonx1   xor()   448 MB/s

[    1.087369] raid6: neonx2   gen()   657 MB/s

[    1.155384] raid6: neonx2   xor()   563 MB/s

[    1.223366] raid6: neonx4   gen()   815 MB/s

[    1.291349] raid6: neonx4   xor()   602 MB/s

[    1.359332] raid6: neonx8   gen()   498 MB/s

[    1.427342] raid6: neonx8   xor()   441 MB/s

[    1.427370] raid6: using algorithm neonx4 gen() 815 MB/s

[    1.427389] raid6: .... xor() 602 MB/s, rmw enabled

[    1.427407] raid6: using intx1 recovery algorithm

[    1.432096] mxs-dma 110000.dma-apbh: initialized

[    1.439654] vgaarb: loaded

[    1.440380] SCSI subsystem initialized

[    1.440941] usbcore: registered new interface driver usbfs

[    1.441034] usbcore: registered new interface driver hub

[    1.441159] usbcore: registered new device driver usb

[    1.442987] i2c i2c-0: IMX I2C adapter registered

[    1.443028] i2c i2c-0: can't use DMA, using PIO instead.

[    1.443471] i2c i2c-1: IMX I2C adapter registered

[    1.443509] i2c i2c-1: can't use DMA, using PIO instead.

[    1.443943] i2c i2c-2: IMX I2C adapter registered

[    1.443980] i2c i2c-2: can't use DMA, using PIO instead.

[    1.444724] media: Linux media interface: v0.10

[    1.444813] Linux video capture interface: v2.00

[    1.444922] pps_core: LinuxPPS API ver. 1 registered

[    1.444946] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>

[    1.445001] PTP clock support registered

[    1.446707] NetLabel: Initializing

[    1.446738] NetLabel:  domain hash size = 128

[    1.446758] NetLabel:  protocols = UNLABELED CIPSOv4

[    1.446834] NetLabel:  unlabeled traffic allowed by default

[    1.447549] clocksource: Switched to clocksource mxc_timer1

[    1.540448] VFS: Disk quotas dquot_6.6.0

[    1.540576] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

[    1.555388] NET: Registered protocol family 2

[    1.556299] TCP established hash table entries: 8192 (order: 3, 32768 bytes)

[    1.556405] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

[    1.556544] TCP: Hash tables configured (established 8192 bind 8192)

[    1.556649] UDP hash table entries: 512 (order: 2, 16384 bytes)

[    1.556716] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

[    1.557081] NET: Registered protocol family 1

[    1.557528] RPC: Registered named UNIX socket transport module.

[    1.557560] RPC: Registered udp transport module.

[    1.557580] RPC: Registered tcp transport module.

[    1.557598] RPC: Registered tcp NFSv4.1 backchannel transport module.

[    1.558588] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available

[    1.561530] futex hash table entries: 1024 (order: 4, 65536 bytes)

[    1.561747] audit: initializing netlink subsys (disabled)

[    1.561818] audit: type=2000 audit(1.528:1): initialized

[    1.563074] workingset: timestamp_bits=12 max_order=18 bucket_order=6

[    1.563241] zbud: loaded

[    1.564301] NFS: Registering the id_resolver key type

[    1.564361] Key type id_resolver registered

[    1.564386] Key type id_legacy registered

[    1.564427] nfs4filelayout_init: NFSv4 File Layout Driver Registering...

[    1.564716] fuse init (API version 7.24)

[    1.565001] orangefs_init: called with debug mask: :none: :0:

[    1.565344] orangefs: module version upstream loaded

[    1.565378] SGI XFS with ACLs, security attributes, realtime, no debug enabled

[    1.570959] Key type asymmetric registered

[    1.571003] Asymmetric key parser 'x509' registered

[    1.571111] bounce: pool size: 64 pages

[    1.571191] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)

[    1.571405] io scheduler noop registered

[    1.571446] io scheduler deadline registered

[    1.571498] io scheduler cfq registered (default)

[    1.578537] PCI host bridge /soc/pcie@0x01000000 ranges:

[    1.578577]   No bus range found for /soc/pcie@0x01000000, using [bus 00-ff]

[    1.578623]    IO 0x01f80000..0x01f8ffff -> 0x00000000

[    1.578657]   MEM 0x01000000..0x01efffff -> 0x01000000

[    2.579812] imx6q-pcie 1ffc000.pcie: phy link never came up

[    2.579847] imx6q-pcie 1ffc000.pcie: Link never came up

[    2.583165] imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00

[    2.583199] pci_bus 0000:00: root bus resource [bus 00-ff]

[    2.583227] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]

[    2.583252] pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]

[    2.583884] PCI: bus0: Fast back to back transfers disabled

[    2.584069] PCI: bus1: Fast back to back transfers enabled

[    2.584176] pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]

[    2.584216] pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]

[    2.584251] pci 0000:00:00.0: PCI bridge to [bus 01]

[    2.584563] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt

[    2.587639] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2

[    2.587691] imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware

[    2.595529] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled

[    2.599009] Serial: AMBA driver

[    2.599522] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 26, base_baud = 5000000) is a IMX

[    2.600376] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 297, base_baud = 5000000) is a IMX

[    3.568760] console [ttymxc1] enabled

[    3.574015] [drm] Initialized drm 1.1.0 20060810

[    3.579865] Error: Driver 'tfp410' is already registered, aborting...

[    3.590308] imx-ipuv3 2400000.ipu: IPUv3H probed

[    3.596995] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    3.603672] [drm] No driver support for vblank timestamp query.

[    3.609870] imx-drm display-subsystem: bound imx-ipuv3-crtc.2 (ops ipu_crtc_ops)

[    3.617550] imx-drm display-subsystem: bound imx-ipuv3-crtc.3 (ops ipu_crtc_ops)

[    3.625232] imx-drm display-subsystem: bound imx-ipuv3-crtc.6 (ops ipu_crtc_ops)

[    3.632914] imx-drm display-subsystem: bound imx-ipuv3-crtc.7 (ops ipu_crtc_ops)

[    3.640421] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    3.649405] imx-drm display-subsystem: master bind failed: -517

[    3.655424] imx-ipuv3 2800000.ipu: IPUv3H probed

[    3.662062] usbcore: registered new interface driver dln2

[    3.668434] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024

[    3.676422] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480

[    3.684477] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000

[    3.692701] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000

[    3.703229] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled

[    3.710274] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode

[    3.719114] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst

[    3.729713] scsi host0: ahci-imx

[    3.733401] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 300

[    3.745163] 2188000.ethernet supply phy not found, using dummy regulator

[    3.760062] pps pps0: new PPS source ptp0

[    3.764729] fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00

[    3.774720] fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: da:e3:c7:4b:7b:9d

[    3.789070] libphy: fec_enet_mii_bus: probed

[    3.794026] fec 2188000.ethernet eth0: registered PHC device 0

[    3.803014] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

[    3.809664] ehci-pci: EHCI PCI platform driver

[    3.814262] ehci-platform: EHCI generic platform driver

[    3.819905] ehci-omap: OMAP-EHCI Host Controller driver

[    3.825411] tegra-ehci: Tegra EHCI driver

[    3.830354] usbcore: registered new interface driver usb-storage

[    3.844834] 2184200.usb supply vbus not found, using dummy regulator

[    3.855195] ci_hdrc ci_hdrc.1: EHCI Host Controller

[    3.860177] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

[    3.875586] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

[    3.881285] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

[    3.888126] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

[    3.895397] usb usb1: Product: EHCI Host Controller

[    3.900309] usb usb1: Manufacturer: Linux 4.6.3-armv7-x4 ehci_hcd

[    3.906437] usb usb1: SerialNumber: ci_hdrc.1

[    3.911651] hub 1-0:1.0: USB hub found

[    3.915477] hub 1-0:1.0: 1 port detected

[    3.920603] using random self ethernet address

[    3.925111] using random host ethernet address

[    3.930232] usb0: HOST MAC 92:7d:b6:32:7a:a7

[    3.934628] usb0: MAC ae:9f:38:42:fb:1a

[    3.938558] using random self ethernet address

[    3.943049] using random host ethernet address

[    3.947636] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008

[    3.954299] g_ether gadget: g_ether ready

[    3.961862] mousedev: PS/2 mouse device common for all mice

[    3.971053] snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0

[    3.980806] i2c /dev entries driver

[    3.988478] coda 2040000.vpu: Direct firmware load for vpu_fw_imx6q.bin failed with error -2

[    3.997092] coda 2040000.vpu: Direct firmware load for v4l-coda960-imx6q.bin failed with error -2

[    4.002137] watchdog: Invalid min and max timeout values, resetting to 0!

[    4.002556] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=1)

[    4.003417] sdhci: Secure Digital Host Controller Interface driver

[    4.003419] sdhci: Copyright(c) Pierre Ossman

[    4.003997] Synopsys Designware Multimedia Card Interface Driver

[    4.004760] sdhci-pltfm: SDHCI platform and OF driver helper

[    4.005569] sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode

[    4.005594] sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO

[    4.005608] sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO

[    4.051724] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

[    4.054261] sdhci-esdhc-imx 219c000.usdhc: could not get ultra high speed state, work on normal mode

[    4.054285] sdhci-esdhc-imx 219c000.usdhc: Got CD GPIO

[    4.055192] ata1: SATA link down (SStatus 0 SControl 300)

[    4.055225] ahci-imx 2200000.sata: no device found, disabling link.

[    4.055231] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug

[    4.101019] coda 2040000.vpu: firmware request failed

[    4.103730] mmc1: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

[    4.107287] ledtrig-cpu: registered to indicate activity on CPUs

[    4.107378] hidraw: raw HID events driver (C) Jiri Kosina

[    4.107962] usbcore: registered new interface driver usbhid

[    4.107964] usbhid: USB HID core driver

[    4.108187] ashmem: initialized

[    4.130679] mmc0: new high speed SDHC card at address aaaa

[    4.131390] mmcblk0: mmc0:aaaa SU04G 3.69 GiB (ro)

[    4.133602]  mmcblk0: p1 p2

[    4.142990] NET: Registered protocol family 10

[    4.147897] mip6: Mobile IPv6

[    4.147912] NET: Registered protocol family 17

[    4.148028] Key type dns_resolver registered

[    4.148038] mpls_gso: MPLS GSO support

[    4.152106] ThumbEE CPU extension supported.

[    4.152126] Registering SWP/SWPB emulation handler

[    4.153049] registered taskstats version 1

[    4.153213] zswap: loaded using pool lzo/zbud

[    4.188551] Btrfs loaded

[    4.192505] Key type encrypted registered

[    4.200478] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    4.207153] [drm] No driver support for vblank timestamp query.

[    4.213334] imx-drm display-subsystem: bound imx-ipuv3-crtc.2 (ops ipu_crtc_ops)

[    4.220987] imx-drm display-subsystem: bound imx-ipuv3-crtc.3 (ops ipu_crtc_ops)

[    4.228621] imx-drm display-subsystem: bound imx-ipuv3-crtc.6 (ops ipu_crtc_ops)

[    4.236245] imx-drm display-subsystem: bound imx-ipuv3-crtc.7 (ops ipu_crtc_ops)

[    4.243754] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    4.252778] imx-drm display-subsystem: master bind failed: -517

[    4.261264] input: gpio-keys as /devices/soc0/gpio-keys/input/input0

[    4.267964] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)

[    4.270675] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    4.270678] [drm] No driver support for vblank timestamp query.

[    4.270867] imx-drm display-subsystem: bound imx-ipuv3-crtc.2 (ops ipu_crtc_ops)

[    4.271020] imx-drm display-subsystem: bound imx-ipuv3-crtc.3 (ops ipu_crtc_ops)

[    4.271189] imx-drm display-subsystem: bound imx-ipuv3-crtc.6 (ops ipu_crtc_ops)

[    4.271341] imx-drm display-subsystem: bound imx-ipuv3-crtc.7 (ops ipu_crtc_ops)

[    4.271374] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    4.272219] imx-drm display-subsystem: master bind failed: -517

[    4.333417] sr_init: No PMIC hook to init smartreflex

[    4.338699] sr_init: platform driver register failed for SR

[    4.344367] of_cfs_init

[    4.346863] of_cfs_init: OK

[    4.362006] usb_otg_vbus: disabling

[    4.365590] CAN XCVR: disabling

[    4.395345] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

[    4.399605] usb 1-1: new high-speed USB device number 2 using ci_hdrc

[    4.410057] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.

[    4.418309] devtmpfs: mounted

[    4.423434] Freeing unused kernel memory: 2048K (c1300000 - c1500000)

[    4.532164] usb 1-1: New USB device found, idVendor=0424, idProduct=2513

[    4.538944] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0

[    4.546985] hub 1-1:1.0: USB hub found

[    4.550898] hub 1-1:1.0: 3 ports detected

[    4.559459] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    4.566165] [drm] No driver support for vblank timestamp query.

[    4.572517] imx-drm display-subsystem: bound imx-ipuv3-crtc.2 (ops ipu_crtc_ops)

[    4.580215] imx-drm display-subsystem: bound imx-ipuv3-crtc.3 (ops ipu_crtc_ops)

[    4.587862] imx-drm display-subsystem: bound imx-ipuv3-crtc.6 (ops ipu_crtc_ops)

[    4.595520] imx-drm display-subsystem: bound imx-ipuv3-crtc.7 (ops ipu_crtc_ops)

[    4.603048] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    4.612156] imx-drm display-subsystem: master bind failed: -517

[    4.748454] systemd[1]: System time before build time, advancing clock.

[    4.862592] random: systemd urandom read with 10 bits of entropy available

[    4.891983] systemd[1]: systemd 229 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ -LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN)

[    4.910656] systemd[1]: Detected architecture arm.

[    4.917985] systemd[1]: Set hostname to <arm>.

[    5.314497] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.

[    5.322276] systemd[1]: Listening on udev Kernel Socket.

[    5.328111] systemd[1]: Listening on Syslog Socket.

[    5.333356] systemd[1]: Reached target Encrypted Volumes.

[    5.339333] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.

[    5.347690] systemd[1]: Reached target Remote File Systems (Pre).

[    5.355064] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.

[    5.364985] systemd[1]: Listening on Journal Socket (/dev/log).

[    5.371850] systemd[1]: Created slice System Slice.

[    5.377537] systemd[1]: Created slice system-getty.slice.

[    5.383317] systemd[1]: Reached target Remote File Systems.

[    5.389607] systemd[1]: Created slice User and Session Slice.

[    5.395758] systemd[1]: Reached target Slices.

[    5.400918] systemd[1]: Created slice system-serial\x2dgetty.slice.

[    5.407895] systemd[1]: Listening on Journal Audit Socket.

[    5.413744] systemd[1]: Reached target Swap.

[    5.418511] systemd[1]: Listening on udev Control Socket.

[    5.424433] systemd[1]: Listening on Journal Socket.

[    5.456233] systemd[1]: Starting Load Kernel Modules...

[    5.465588] systemd[1]: Starting Journal Service...

[    5.491211] systemd[1]: Mounting Debug File System...

[    5.500548] systemd[1]: Started Read required files in advance.

[    5.511204] systemd[1]: Mounting POSIX Message Queue File System...

[    5.522318] systemd[1]: Starting Create list of required static device nodes for the current kernel...

[    5.536185] systemd[1]: Starting Remount Root and Kernel File Systems...

[    5.547036] systemd[1]: Starting Nameserver information manager...

[    5.554386] systemd[1]: Started Forward Password Requests to Wall Directory Watch.

[    5.572682] systemd[1]: Started Load Kernel Modules.

[    5.595953] systemd[1]: Started Remount Root and Kernel File Systems.

[    5.620158] systemd[1]: Started Create list of required static device nodes for the current kernel.

[    5.681884] systemd[1]: Starting Create Static Device Nodes in /dev...

[    5.695795] systemd[1]: Starting Load/Save Random Seed...

[    5.727763] systemd[1]: Starting udev Coldplug all Devices...

[    5.738779] systemd[1]: Mounting FUSE Control File System...

[    5.750090] systemd[1]: Mounting Configuration File System...

[    5.765756] systemd[1]: Starting Apply Kernel Variables...

[    5.783235] systemd[1]: Mounted POSIX Message Queue File System.

[    5.789970] systemd[1]: Mounted Debug File System.

[    5.795328] systemd[1]: Mounted FUSE Control File System.

[    5.801388] systemd[1]: Mounted Configuration File System.

[    5.808556] systemd[1]: ureadahead.service: Main process exited, code=exited, status=5/NOTINSTALLED

[    6.669770] /panel: could not find display-timings node

[    6.675184] panel panel: could not get panel timings

[    6.694900] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    6.710744] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    6.931941] etnaviv-gpu 2204000.gpu: hw init failed: -6

[    6.947711] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    6.962351] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    7.022422] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    7.028319] imx-sgtl5000 sound: ASoC: CODEC DAI sgtl5000 not registered

[    7.028327] imx-sgtl5000 sound: snd_soc_register_card failed (-517)

[    7.126127] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    7.161908] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

[    7.183703] imx-drm display-subsystem: failed to bind display@di0 (ops imx_pd_ops): -517

Press Enter for maintenance

(or press Control-D to continue):

root@arm:~# apt-get update

Reading package lists... Done

E: List directory /var/lib/apt/lists/partial is missing. - Acquire (30: Read-only file system)

W: Not using locking for read only lock file /var/lib/dpkg/lock

root@arm:~#

ラベル(3)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,569件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi VENKATA

please check

https://boundarydevices.com/compiling-latest-u-boot-for-i-mx6-2015-edition/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,569件の閲覧回数
venkatachilakal
Contributor III

Hello igorpadykov,

Thank you very much for your support..  I need one more help in u-boot upgrading.

I have downloaded the 6x_upgrade and u-boot.nitrogen6q files to sd card.

As per the blog, we need to run the following commands from the U-boot command line.

bootfile=u-boot.nitrogen6q ; run upgradeu

But, this this upgradeu command is not supported by my current u-boot version.

My Current U-Boot Version : 2014.04-00123-g63ae4a5 (May 14 2014 - 17:09:55)

As per blog I have to upgrade this to 2015 Version.

So, please guide me to upgrade my u-boot version.

Thank you very much once again for your support.

0 件の賞賛
返信

2,569件の閲覧回数
venkatachilakal
Contributor III

I just downloaded the 6x_upgrade script and u-boot.nitrogen6q files from here​.

Then I followed below steps...

Format microSD/SD card:

export DISK=/dev/sdb

Erase microSD/SD card:

sudo dd if=/dev/zero of=${DISK} bs=1M count=30

Create Partition Layout:

sudo sfdisk --in-order --Linux --unit M ${DISK} <<-__EOF__

1,20,0x83,-

__EOF__

Format Partitions:

sudo mkfs.ext2 ${DISK}1 -L boot

Mount Partitions:

On some systems, these partitions may be auto-mounted...

sudo mkdir -p /media/boot/

sudo mount ${DISK}1 /media/boot/

Copy Factory Images to microSD/SD card:

sudo cp -v u-boot.nitrogen6q /media/boot/u-boot.imx

Remove microSD/SD card:

sync

sudo umount /media/boot

using: microSD media

setenv mmcdev 1

Loading u-boot.imx to Flash

mmc dev ${mmcdev}

ext2load mmc ${mmcdev}:1 0x10800000 u-boot.imx

sf probe 1 27000000

sf erase 0 0xc0000

sf write 0x10800000 0x400 ${filesize}

But, I got error

Here is the log

U-Boot > sf erase 0 0xc0000

SF: 786432 bytes @ 0x0 Erased: ERROR

U-Boot > sf write 0x10800000 0x400 ${filesize}

SF: 461824 bytes @ 0x400 Written: ERROR

So, How can I upgrade my u-boot.... Please help me

0 件の賞賛
返信