No thorough battery tests have been ever done on the i.MX6 SABRE SD board. The board provides two MAX8903 battery charger/power manager ICs and can operate two regular one cell 3.7V Li-ION batteries, one battery per MAX8903 IC.
There are two regular 0.1" pitch 4-pin single row connectors (one male, one female) provided on the board, they are connected in parallel. They are referenced as CON2 and CON3, please refer to the board schematics.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------