Sabre-AI external mudules

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre-AI external mudules

ソリューションへジャンプ
4,153件の閲覧回数
JHY
Contributor IV

Sabre-AI board has external module connectors for GPS, Bluetooth, WiFi.

Are there recomended devices or information for those modules?

ラベル(1)
1 解決策
4,026件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Yes, software support is same for both.

Michal

元の投稿で解決策を見る

4 返答(返信)
4,026件の閲覧回数
art
NXP Employee
NXP Employee

The following WiFi/BT components have been tested on both SABRE-SD and SABRE-AI boards.

1. SDIO cards based on the Atheros AR6103 802.11 b/g/n single-chip WiFi solution.

2. SX-SDCAN 802.11a/b/g/n + BT SDIO Card by Silex, based on the Qualcomm Atheros AR6233 single-chip solution.

3. The solutions based on the BCM4339 chip by Broadcom.

Regarding GPS, generally, any GPS chipset that supports NMEA protocol through

the UART interface can be used. The tested solution is the AR1520A chipset from Atheros.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,026件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Hi JHY,

as GPS you can use any GPS module connected over UART. In Linux are drivers for this. For BT/WiFi are preferred Atheros chips for ex.: SX-SDCAN | SDIO Radios | Silex Technology America

Hope it helps

Michal

4,026件の閲覧回数
JHY
Contributor IV

Silex BT/Wifi is mentioned in SABRE-SDP documents.

Is it same for SABRE-AI?

0 件の賞賛
返信
4,027件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Yes, software support is same for both.

Michal