Saber-SD Quad Android Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Saber-SD Quad Android Performance

1,367 Views
chuck_ferguson
Contributor I

Performance issue...

I have three Android tablets:

1. Saber-SD board with i.mx6 quad processor.

2. a dinky single-board computer with Samsung exynos 5422 processor (Odroid XU4).

3. industrial tablet running Intel N4200 ApolloLake processor.

All of them are on the same network. They all have about the same memory.

The i.mx6 is significantly slower than others. Significantly. YouTube videos look like they are running at reduced frame rate. Google Maps updates are slow enough to see individual map tiles populating the screen. I was expecting comparable performance from the imx6, especially when compared to the hobby-grade Odroid.

I thought the imx6 might be self-throttling for thermal management. So I attached a heat sink. No improvement.

I can't tell if the processor itself is slow or its network hardware. It is definitely not the LAN since all 3 boards are on the same LAN.

Any thoughts? How can I tell if all 4 processors are running? Anything special I need to do in Uboot or otherwise to crank up the performance?

Thanks in advance,

Chuck

Labels (3)
0 Kudos
Reply
1 Reply

1,283 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Chuck,

You would need to compare the characteristics of each of the three tablets as there are many factors that may affect performance.

You can see the CPUs running and at which speed by using the command:

$ cpufreq-info

There is also information available on /sys/devices/system/cpu that may be of help.

I would check this information in the three boards and also take into account the kind of core of each tablet and available RAM, Android version running etc.

I hope this helps!

Regards,

0 Kudos
Reply