SRK table generation with HSM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRK table generation with HSM

2,464件の閲覧回数
rohith_chinnasw
Contributor II

We are using the CST tools 3.1.0 version and have customized the backend to sign the bootloader HAB images. But as part of it the input to the signing process is an SRK table bin file and it looks to be using the private keys to generate it. Since we have the private keys in the HSM is it possible with CST tool to use the HSM backend for the SRK table generation as well?

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,360件の閲覧回数
PramodKumar
Contributor IV

Hello Rohith chinnaswamy ,

Are you doing the code signing with imx6ul or any other .

Have a great day ,

Pramod

0 件の賞賛
返信

2,360件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

     Please look at  "cst-3.1.0.tar\release\code\back_end-hsm\doc\" .

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信