SRAM usage by the ROM bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRAM usage by the ROM bootloader

ソリューションへジャンプ
2,414件の閲覧回数
stefano-quantic
Contributor III

I'm using iMXRT1176.
I need to store some values in SRAM, and be able to retrieve them after a (non-power-cycle) reset.
I need to know which parts of SRAM could be touched by the ROM bootloader, so that I can allocate my variables at different addresses.
The reference manual (§10.5.1 "Internal ROM/RAM memory map") states that a portion of OCRAM1 is used: 0x20240000-0x2024FFFF
Is it correct that this is the only portion of SRAM that is modified by the bootloader?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,348件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @stefano-quantic,

We apologize for the delay to get back to you.

As the i.MX RT1170 Processor Reference Manual. Section 10.5.1 Internal ROM/RAM memory map mentions: "The RAM space occupied by ROM cannot be used as part of the boot image. The entire OCRAM1 region can be used freely after the boot. The above OCRAM1 region must be reserved if the user application needs to call the HAB API/FlexSPI NOR API for image authentication."

The reference manual (§10.5.1 "Internal ROM/RAM memory map") states that a portion of OCRAM1 is used: 0x20240000-0x2024FFFF

Finally, we just like to point out that according the i.MX RT1170 Processor Reference Manual., OCRAM1 region is from 0x2024_0000 to 0x2024_BFFF.

Best regards, Raul.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,349件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @stefano-quantic,

We apologize for the delay to get back to you.

As the i.MX RT1170 Processor Reference Manual. Section 10.5.1 Internal ROM/RAM memory map mentions: "The RAM space occupied by ROM cannot be used as part of the boot image. The entire OCRAM1 region can be used freely after the boot. The above OCRAM1 region must be reserved if the user application needs to call the HAB API/FlexSPI NOR API for image authentication."

The reference manual (§10.5.1 "Internal ROM/RAM memory map") states that a portion of OCRAM1 is used: 0x20240000-0x2024FFFF

Finally, we just like to point out that according the i.MX RT1170 Processor Reference Manual., OCRAM1 region is from 0x2024_0000 to 0x2024_BFFF.

Best regards, Raul.

0 件の賞賛
返信