SPL to be signed ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPL to be signed ?

4,198 次查看
antonio_santagi
Contributor IV

Hello ,

I am using iMX8M mini.

I am following the CST code signing tool and the document https://www.nxp.com/docs/en/application-note/AN4581.pdf 

These documents talks about signing u-boot.imx , but what about the SPL ? Does it need to be signed and with IVT and other info table ( imx format ) as well as u-boot does ?

Do instead the docs mean an all inclusive u-boot meaning u-boot+spl ?

thank you

标记 (3)
0 项奖励
回复
5 回复数

4,048 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Antonio

>Do instead the docs mean an all inclusive u-boot meaning u-boot+spl ?

right. AN4581 was written when spl was not supported with i.mx processors.

In general more updated documentation can be found on

imx\doc - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,049 次查看
antonio_santagi
Contributor IV

Thank you that is useful. Which is the command to configure and then build U-boot from those sources for the imx8mm_vk ?

0 项奖励
回复

4,049 次查看
igorpadykov
NXP Employee
NXP Employee

please look at tutorial on

imx\doc - uboot-imx - i.MX U-Boot 

"Step-by-step guides are available under doc/imx/habv4/guides/ directory"

introduction_habv4.txt\habv4\imx\doc - uboot-imx - i.MX U-Boot 

Best regards
igor

0 项奖励
回复

4,049 次查看
antonio_santagi
Contributor IV

thank you,

I completed the part described on that document and

at the end of that document I can read

The SRK_1_2_3_4_table.bin and SRK_1_2_3_4_fuse.bin files can be used in further steps as explained in HAB guides available under doc/imx/habv4/guides/ directory.

But I cannot find any other document that follows with other steps required to build imx8mm_evk U-boot.

I was expecting to find somewhere where it explains how to configure for the board like "make imx8mm_evk_defconfig "or something similar , but I cannot find it. 

0 项奖励
回复

4,049 次查看
igorpadykov
NXP Employee
NXP Employee

additional document was sent vial mail.

~igor

0 项奖励
回复