SPL must contain the NAND Driver and UBIFS file system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPL must contain the NAND Driver and UBIFS file system

1,718 Views
adityanagal
Contributor III

Hi ,

If the SPL and uboot resides  in the NAND flash. Question is , does the SPL have the NAND FIash driver and the UBIFS file system. As per the below thread , I was suggested these should not , but per my understanding , when the SPL executes in SRAM , how will it loads the uboot  from NAND FLash unless it has the NAND Flash Driver and UBIFS file system. Please suggest.

https://community.nxp.com/thread/451729

Regards,

Aditya Nagal

0 Kudos
Reply
3 Replies

1,467 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

NAND Flash Driver and UBIFS file system are attributes of operating system,

while uboot is baremetal, just  executing instructions as binaries.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,467 Views
adityanagal
Contributor III

Hi igor ,

Thank you for your response  , I have small disagreement with you on this point as though uboot  is a bare metal code , it has the layers of drivers and file system. Without these layers , how would SPL loads the uboot from Nand Flash and uboot loads the kernel from Nand Flash. In the uboot source, at path uboot/drivers , all drivers are  listed. Similarly at path uboot/fs , all supported file systems are listed. Now just the question is , how to configure u-boot with a particular file system UBIFS  . Also ,  how to configure SPL with MTD flash driver and UBIFS file system. Need your suggestion on this.

Regards,

Aditya Nagal

0 Kudos
Reply

1,467 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

 

please check

https://en.wikipedia.org/wiki/Das_U-Boot
U-Boot does not need to be able to read a filesystem in order for the kernel to use it
as a root filesystem or initial ramdisk; U-Boot simply provides an appropriate parameter to the
kernel, and/or copies the data to memory without understanding its contents.

regarding uboot ubifs support, seems this depends on architecture/version:
http://www.denx.de/wiki/publish/DULG/DULG-enbw_cmc.html#Section_5.9.3.6.
https://stackoverflow.com/questions/39582079/enabling-ubifs-in-u-boot

as for SPL, I am afraid it does not support ubifs, for more info one may post this on uboot mail list

U-Boot Info Page 

note, nxp uboot does not support spl.

 

Best regards
igor

0 Kudos
Reply