SPL is failing because of new memory and size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPL is failing because of new memory and size

1,955 Views
srinivasaporam
Contributor II

Hi,

We have got  customized board based on reference design of IMX6QDL . Difference is memory technology. Reference board is DDR3 (1GB) where as new board is LPDDR2 (512MB). We are Denx u-boot source for building. Can anybody guide us what are all the files those we need to modify.

We have some technical literature (attached) which states that if RAM is new SPL will fail.

can anybody tell us all files those need to be changed.

Labels (2)
0 Kudos
Reply
1 Reply

1,824 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

for different memory it may be necessary for to modify CONFIGs, please refer to attached README

and look at

Wandboard - Freescale i.MX6 ARM Cortex-A9 Community Development Board - December 26 2013 - Introduci...

Wandboard - Introducing SPL u-boot for the #wandboard... | Facebook

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply