SPL code, pmic_stby_req

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPL code, pmic_stby_req

1,338件の閲覧回数
sbmd_1234
Contributor III

Hi 

I have read the spl.c code inside power_init_board() function reg_write is happening as : 

/* BUCKxOUT_DVS0/1 control BUCK123 output */
pmic_reg_write(dev, PCA9450_BUCK123_DVS, 0x29);

/* enable DVS control through PMIC_STBY_REQ */
pmic_reg_write(dev, PCA9450_BUCK1CTRL, 0x59);

So, what i understood is like in every board bootup register write of DVS controlling through pmic_stby_req  is configured of PMIC.

But my question is how the system is getting triggered when the imx93 is sending standby request?

0 件の賞賛
返信
2 返答(返信)

1,316件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @sbmd_1234 

 

When the PMIC receives the standby request signal PMIC_STBY_REQ it interprets this signal as a request to transition the system into a low-power state.

Also you can check the reference manual, look the PMIC standby control (PMIC_CTRL) register and PMIC standby pre delay control (PMIC_PRE_DLY_CTRL).

 

Best regards.

0 件の賞賛
返信

1,314件の閲覧回数
sbmd_1234
Contributor III

Hi @Manuel_Salas 

Thanks for your reply!!

Actually, I can see the system gets voltage down by the PMIC i.e ( BUCK1_VOUT_DVS1 reg) during booting time but the question is may be somewhere system checks the low power mode conditions so can we read those conditions.

If those conditions are checked for standby then what is that process?

 

0 件の賞賛
返信