SPL bootup issue for IMX7D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPL bootup issue for IMX7D

154 次查看
patrickzhang1024
Contributor II

Hi,

    I have an issue with SPL boot up. I am currently using fastboot eMMC in uboot and uuu tools for loading. I loaded SPL into bootloader0 which is 0x2 block in boot partition. The normal u-boot used to be loaded to that place as well.

The command I use is "FB[-t 60000]: flash bootloader0 SPL" , but there are nothing showing when device restart and seems bootROM can't find the image.

The SPL image has the IVT header and DCD, the CSF security stuff is disabled. 

If I use "DP: boot -f SPL", I can see that SPL is running in RAM.

Does anyone have idea that will it can't boot from eMMC?

 

The attach file is SPL.imx. I rename it to .bin for upload.

#imx #uboot

 

0 项奖励
回复
1 回复

102 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI @patrickzhang1024 

Please share  your UUU script file.

B.R

0 项奖励
回复